11/15/2018 12:43 PM | |
Joined: 11/29/2011 Last visit: 10/25/2023 Posts: 1348 Rating: (228) |
Hi, I was wondering if anyone had experience with working on PCS7 projects remotely. What I need is to set up a home office where from I can do a few days of work every week. Something like setting up a VPN connection to an ES or something like that. I have a seen a few examples of Remote Services, but I was wondering if someone have first hand experience. How well this works? I am looking forward your comments on this topic! |
- What you read here, please check with manuals and your requirements. |
|
11/15/2018 1:09 PM | |
Joined: 3/14/2008 Last visit: 3/28/2024 Posts: 2059 Rating: (924)
|
Hi Microman, I have used this scenario. My system was as follows: We have a virtual machine (ESX) with a virtual ES and OS on it. In order to connect to them, we have a thin client. On the thin client is RealVNC installed, so we can take over ES and OS. At home, I made a connection with the thin client over VPN. This way, we had no additional software running on the ES and OS... |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on