12/7/2018 1:31 PM | ||||
Posts: 11 Rating: (0) |
I've done everything according to the manual(as you wrote above) and as I said, Webserver works fine so for me Logo comfort should work as well. I also installed the Logo App and there is also everything fine! I can connect to the controller with no issues. I got my Logo comfort on a CD so it is full and legal. I tried on different PC with no luck |
|||
This contribution was helpful to1 thankful Users |
12/7/2018 6:51 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
Please write us the type of the TP link router. |
12/8/2018 10:12 AM | |
Posts: 11 Rating: (0) |
tp-link TL-WR841N ver 13 300Mbps Wireless N Router |
1/24/2019 3:02 PM | |
Joined: 7/28/2007 Last visit: 7/31/2024 Posts: 29 Rating: (2) |
I suggest you to test port 102 or 103. For me was OK on Logo7. |
4/21/2019 12:38 AM | |
Posts: 1 Rating: (0) |
Hello Finally, I can connect with DNS, I can help yo |
Follow us on