11/23/2018 8:14 AM | |
Joined: 9/19/2011 Last visit: 4/8/2024 Posts: 32 Rating: (0) |
Dear I use the follow systems: - WinCC V7.4 Upd 8 - PCS 7 V9.0 SP1 First thing, you need to now is that the horn is controlled by the PLC (Q38.7) and that we doesn't use the sound card. The installation consists of redundant servers, OS-Client and an engineering station. So i configured the horn like the screenshot in the attachment. I tested the connection between PCS7 and WinCC. If i use an button on a screen and i configure the left button of the mouse so that if i push the left button sent a 1 to the OP_D block in the CFC it works perfect and if i use the rigth button a 0 is sent to the OP_D block. But if a alarm is triggerd, the OP_D block doesn't do anything. Did i configure something wrong? In my opinion it should be work but of course I am not an expert. I hope somebody can help me. In the meantime I have tried hundreds of things without results. Kind regards Frederik Van Rompaey
AttachmentProbleem Piloot.zip (76 Downloads) |
11/27/2018 4:46 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Are you sure, that you have installed WinCC V7.4 Upd8? (not compatible with PCS 7 V9.0 SP1) I think, you have installed WinCC V7.4 SP1 Upd8 (compatible with PCS 7 V9.0 SP1) |
SIMATIC PCS 7 - Overview |
|
12/13/2018 10:53 PM | |
Joined: 9/19/2011 Last visit: 4/8/2024 Posts: 32 Rating: (0) |
I looked at this link: https://support.industry.siemens.com/cs/ww/en/view/109756832 The horn still doesn’t work with the horn configurator. I have a script that triggers my horn if the group display gives an alarm, warning,... The only problem i have is that if i had an alarm and i acknowledge the horn, the horn stops but if te same alarm disapear and triggers again without ackn the alarm message, the horn is working again. In the horn configurator you have a option to not trigger if alarm isn’t achnowledged. I don’t kwon how to write this in the script. On the groupdisplays you have no distincion between alarms. An alarm is the hex value D000. For every warning is thus the same value. Otherwise i had could made an alarm storage and i could see the difference between the current value and the value before. I also send the program to Siemens but they can’t find the problem. It’s something strange. |
Last edited by: Jen_Moderator at: 12/14/2018 11:59:57 AMOptimized link. |
|
Follow us on