12/14/2018 10:31 AM | |
Joined: 10/23/2015 Last visit: 2/18/2024 Posts: 159 Rating: (2) |
Dear all, I would like to move a DWord type to a UDT (of 4 bytes), is it possible ? Thanks |
12/14/2018 11:16 AM | |
Joined: 5/6/2010 Last visit: 3/27/2024 Posts: 1954 Rating: (266) |
Hello ahi_77, yes, you can do this. You should use the command AT. Please look at this FAQ - 57132240, there is a description to use the AT-command.
|
12/14/2018 11:49 AM | |
Joined: 10/23/2015 Last visit: 2/18/2024 Posts: 159 Rating: (2) |
Hello thanks you, And i use an FC (without static) ? BR |
Follow us on