12/19/2018 3:36 PM | |
Posts: 2 Rating: (0) |
Hello Everybody, I try to set up a PROFIsafe connection, by using a CP1616 and ET200SP(CPU 1512SP F-1 PN/ 6ES7 512-1SK01-0AB0 / Firmware V2.1 ). When I go online i keep receiving this error message "IO device failure - Differing device type". IP addressis good, Cables are plugged properly. I attached multiple screenshots and a Diagnostic.txt file. Thank you AttachmentPS.zip (224 Downloads) |
12/25/2018 12:40 PM | |
Posts: 64 Rating: (4) |
1) check modules type in the ET200SP rack 2) check the firmware version of the modules; |
1/5/2019 1:30 PM | |
Posts: 64 Rating: (4) |
From your printscreen I can see that you don't have connection to CP1616 device. That's why you have error. |
Follow us on