6/9/2018 8:43 AM | |
Joined: 1/14/2018 Last visit: 2/28/2024 Posts: 9 Rating: (1) |
hi friend ; please can u tell me which buffer battery u mean ? in the PS ? |
12/22/2018 9:04 AM | |
Joined: 11/6/2018 Last visit: 8/14/2023 Posts: 9 Rating: (0) |
Hi If I was to click on the Update button on the attachment would the extf go away on the CPU? |
12/26/2018 11:58 AM | |
Joined: 1/14/2018 Last visit: 2/28/2024 Posts: 9 Rating: (1) |
which battrey buffer you mean ? can u explain ? |
12/26/2018 8:23 PM | |
Joined: 1/14/2018 Last visit: 2/28/2024 Posts: 9 Rating: (1) |
which battery buffer please ? |
12/26/2018 8:29 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066) |
There is only one battery backup. And this one is in the power supply. |
Follow us on