2/11/2019 6:33 AM | |
Joined: 10/14/2014 Last visit: 9/6/2024 Posts: 26 Rating: (0) |
Similar problem. At some point in time, the 3RW44 is reset to the factory settings: a window appears with a choice of interface language and sequential input of parameters (application, load current, etc.). After confirming that the settings have been saved, everything repeats again. The problem was solved as follows: the OK button was pressed very quickly for a few seconds or minutes and this cycle was interrupted once. The initial settings are preserved and other parameters could be entered. This problem has already occurred more than once on different devices of the same type 3RW 4436. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/11/2019 1:20:27 PMNew subject after splitting |
|
2/11/2019 1:54 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Spontaneous reset 3rw44 is published within the conference Industrial Controls.
Jen_Moderator |
Follow us on