4/11/2018 6:58 PM | |
Joined: 3/10/2011 Last visit: 4/27/2023 Posts: 27 Rating: (0) |
When I compare online / offline, get differences in a block that uses pointers (parameters for BLKMOV SFC20). The ladder shows the same address in both online and offline but the result box shows different addresses (not even the same format). How do I keep this from happening? Result box has the following for example: Offline Network 9 SFC 20 - Formal parameter SCRBLK: P#DB72.DBX100.0 BYTE 32 Online Network 9 SCRBLK: 16#84000320 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/12/2018 11:05:21 AMNew subject after splitting |
|
4/12/2018 12:22 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi, can you show us a screenshot of the behaviour? regards, |
FCK WAR! |
|
4/13/2018 8:32 AM | |
Joined: 2/11/2015 Last visit: 9/19/2024 Posts: 464 Rating: (34) |
Hi, Online is directly the value of the pointer. Pay attention at the FORMAT you visualize the online values. |
7/9/2018 7:19 PM | |
Joined: 3/10/2011 Last visit: 4/27/2023 Posts: 27 Rating: (0) |
It seems this is also present in TIA/Portal. This is not a pointer as I had seen in Step 7 but the compare shows differences where there aren't any. If you look at the addresses, they are the same, but online program is displayed using a different format, so basically the same question - how to avoid erroneous results. Attachmentsiemsimpossible1.docx (127 Downloads) |
Follow us on