2/14/2019 2:36 AM | |
Joined: 9/28/2017 Last visit: 9/23/2024 Posts: 3 Rating: (0) |
Hi, We have a WinCC Server with WinCC v7.2 that we have upgraded to WinCC v7.4. Also the operating system was updated from Windows Server 2008 to Windows Server 2012. Project has been migrated. The WinCC Web Navigator Server has been upgraded by doing this WinCC upgrade. When trying to open the website the client hangs on "No connecting to server". When I check IIS manager, Web Navigator is running. But when I open my project with Web Navigator in other station (PC client), I cannot open my project, Web Navigator cannot Connect to Server. I disabled the firewall, removed the antivirus, tried different versions of Internet Explorer (8,9,10,11; 32x / 64x) on different versions of Windows, tried to re-create the site via the Web Configurator with another port, installed WinCC RT on the client, reinstalled the software. All licenses are ok. Nothing helped. What could be wrong here ? AttachmentDoc2.pdf (208 Downloads) |
Follow us on