2/16/2019 9:17 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32877 Rating: (4064)
|
The fact that you provide us with the program is a prerequisite for accurate help. Otherwise it is only guess ... |
2/16/2019 9:45 PM | |
Joined: 9/29/2014 Last visit: 8/6/2022 Posts: 60 Rating: (1) |
Attachmentweld.machine.zip (144 Downloads) |
2/17/2019 2:17 PM | |
Joined: 5/19/2017 Last visit: 4/16/2024 Posts: 15 Rating: (5) |
I've deleted my previous post, because I read again your description and now I know I missundestood what you want, so I made another version, but I don't understand exactly how would be work tha automatic cycle. But I made this so try it. First you need to use it manual, so you have to press the I1 (Q1 is activated) and after that less than 1 sec the I2 (Q2 will be forbidden) than relase the I1 (Q3 will be activated). And after that the sensor (I3 has to press) sends a signal and the automatic function begins. When you press the I1 again it will stop (Q1,Q2 is stopped) . Attachmentweld_maschine2.zip (149 Downloads) |
2/17/2019 6:28 PM | |
Joined: 9/29/2014 Last visit: 8/6/2022 Posts: 60 Rating: (1) |
it's not what I want thank you for the effort I will try to make it myself and then upload it
|
Follow us on