2/15/2019 8:38 AM | |
Posts: 2 Rating: (0) |
I have a Siemens 3 system machine tool because of long time parameter loss, the PLC program through the AS511 interface card to connect the PLC is also lost. Now the original factory PLC backup, TE% program L program, now the system can start normally after power-on through standard system loading, but the mode selection switch on MCP can not be used, only stay in the MD-SET mode can not be switched on (whether normal). To return the PLC through STEP5, when ALL module is selected for transmission, STEP5 alarm module is in EPROM and transmission is interrupted. Transferring PB FB OB DB separately can be imported, but PC FC cannot. The system can not work properly. How to transmit S5-130W PLC program? How to restore Siemens 3M system? Thank you very much. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/15/2019 1:20:35 PMNew subject after splitting |
|
Follow us on