2/17/2019 5:46 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hi Teo If you want a good answer, you should explain a little better. Once you have an object of Excel with CreateObject then you can save with obj.ActiveWorkbook.SaveAs "C:\Backup\Recipe_No.2_DateTIme" & ".xls" , 56 You can see an spanish sample here, but the code is the same . Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
2/18/2019 1:59 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hi Teo Can you show your hole code to test it? Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
2/18/2019 3:46 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hi Teo Your code is wrong !!! RecipeNo not exist in your code
Try this:
Regards. If this help you, use the rate button, it is free of charge :-) |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on