4/2/2019 12:50 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Actually you should have post your query in Low-Voltage Controls Industrial Controls product conference. Now to your question, your motor capacity is 22.4, 41.6 A, 415 volt. Soft starter cacacity is 110 Kw. Ratio of motor to ss is 1:5. If you connect the motor to this SS, you can not get SS complete protection, so it is not recomanded. General ration of motor to SS is 1-1.10. HTH. |
Follow us on