6/10/2015 7:44 AM | |
Posts: 7 Rating:
|
Dear Support
We are offering a system upgrade to one of our customer in UAE region, this upgrade is from PCS7 V6.1 SP1 to PCS7 Version 8.0 (or whichever is the latest one), this if for Server-4 no’s , OS- 2 No’s and ES- 2 No’s.
Can you please help us in selecting the appropriate upgrades licenses and software required for this migration.
---------------------------------------------------------------------------------------------------- Split from UPGRADE FROM PCS7 6.0 to PCS7 LATEST VERSION (Libraries) |
Last edited by: Min_Moderator at: 6/10/2015 3:10:14 PMNew subject after splitting |
|
6/10/2015 9:16 AM | |
Posts: 26 Rating:
|
You should have the part numbers of existing version or list of all licence installation (Existing) then you can easily find for upgrade licences in CA01. |
6/10/2015 3:43 PM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating:
|
Hello kkhar First upgrade from V6.1 to V7.1 Server:6ES7658-2BX17-0YE0 Client:6ES7652-5CX17-0YE5 Then upgrade from V7.1 to V8.1 (latest version) Server:6ES7652-8BX18-0YE0 Client:6ES7652-8CX18-0YF5 I do not know if you have redundant servers. If so you need different upgrade licenses for V7.1 to V8.1: 6ES7652-3BX18-2YE0. This license is valid for two servers. |
Greetings |
|
This contribution was helpful to
1 thankful Users |
Follow us on