9/17/2015 6:02 PM | |
Joined: 11/7/2014 Last visit: 9/10/2024 Posts: 12 Rating: (1) |
hello everyone, Recently i got into a faulty turning center with 810D CCU3.4 SW VERSION 6.5 and it got exactly the same error as the thread owner's case.
I have checked the following: -Took the faulty machine's PCU into another working machine and it worked. -Put the working machine's CF-card into the faulty one and it didnt work. -Tried booting pressing key "6" to get into Caldera Dos and picked option "-", option "8". Both didnt work. I want to ask a few questions: -how to verify what caused the error black windows with ASCII characters at the bottom? -can i put the CF-card of the faulty machine into a good machine (also turning center but bigger size) to check whether the CF-card is still OK? I am not sure what exactly is wrong so please help, thank you guys. UPDATED: here is a photo of the LEDs when the machine finished booting up with ASCII chars window. What does SF LED mean in this case? a drive error? or CCU error?
------------------------------------------------------------------------------------------ |
Last edited by: quangnguyen,digicnc at: 9/17/2015 6:49:00 PMLast edited by: CS Moderator at: 9/18/2015 10:59:24 AMNew subject after splitting; referenced post inserted |
|
Follow us on