10/20/2015 5:52 PM | |
Joined: 8/15/2015 Last visit: 8/21/2024 Posts: 133 Rating: (4) |
Dear Sir , I would like a small Clarification , Is it posible to conect on a LOGO 8 , Modbus RTU ? If now How can this be made with other ways like Modbus IP , or whatever .. If yes How can it be done ? Thanks !! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/21/2015 11:11:37 AMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
10/21/2015 4:31 PM | |
Posts: 439 Rating: (108) |
Bonjour Le Test !! A cheap way to communicate Modbus RTU would be to go with a S7-1200 and then communicate with you Logo!. Best regards, Hugo |
Follow us on