6/5/2018 10:25 AM | |
Joined: 1/10/2014 Last visit: 10/3/2024 Posts: 7 Rating: (0) |
Dear Friends, we have the 6RA8075-6DV62-0AA0-Z DC Drive. but since installation the drive has failure three times, and every time the thyristor burnt, and this happens at power failure. it happens like machine running well but if there will any power failure than the drive thyristor burnt. three times this had happen. cause is same while power failure than only the thyristor fails. we have placed the MCCB, SITOR Fuses, Choke, Power Contactor, in input side, and for output there are also fuses available for and short circuit or other issues, but fuses find healthy at all the time but thyristor burnt at power failure. this happens at any interval. ------------------------------------------------------------------------------------------ |
Last edited by: Sanjay Sharma at: 6/5/2018 10:29:33 AMLast edited by: Jen_Moderator at: 6/5/2018 12:16:08 PMNew subject after splitting |
|
Follow us on