10/22/2018 8:23 AM | |
Joined: 3/20/2012 Last visit: 8/13/2024 Posts: 118 Rating: (1) |
Hi, I've got a PCMCIA Card (6FC52470AA110AA3) For a CN. How can i read or write it. Is a PG able to? Thanks for help. |
10/23/2018 6:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Which is the system? What you want to read-write? |
10/23/2018 10:42 AM | |
Joined: 3/20/2012 Last visit: 8/13/2024 Posts: 118 Rating: (1) |
A few weeks ago my CN has been stopped due to a problem with a PCMCIA Card ref 6FC5 250-6AX30-5AH0, wich contains licences for 31 axes. The PCMCIA Card was broken. The manufacturer had a backup of the licences and has been able to reconstruc a new PCMCIA Card similar to the first one. Now, i want to be shure to be able to fix this problem if it occurs on an other machine. So i have to read PCMCIA Card and be able to write an empty one (6FC5 247 0AA11 0AA3). Siemens has told me that i will need 2 software: "SINUMOCOM FFS" and "PcCARD". I've got it. I'm equipped with a PG Field M5 6ES7 717-1BB01-0AC0 (Win7). My problem is: when i insert an empty PCMCIA card in the PG card Reader, i don't have any letter (E: for example) appearing. Best regards. |
10/24/2018 8:16 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Are you sure SINUCOPY FFS & PCCARD are compatible with WIN 7 ? |
Follow us on