5/21/2021 6:07 PM | |
Posts: 1 Rating: (0) |
Hello, i have the same type of alarm: 21612 Channel 1 axis S1/B VDI-signal 'drive enable' reset during traverse motion This alarm comes when the spindle decelerates either while changing speeds during automatic cycle or when running the spindle in MDI and pressing RESET. However, if running the spindle at 250rpm, then press RESET, no alarm. Run the spindle 300RPM then press RESET, alarm 21612 appears. After 21612 the alarms 700102 Supply module not ready for operation and 700104 Supervising module not ready for operation appear. On the NCU, only while the spindle is running, there is a amber light that blinks rapidly, then becomes steady on for a few seconds, then starts blinking rapidly again, continuously. The light is beside letters CB. what does this indicate? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2021 08:50:22New subject after splitting |
|
9/10/2021 6:50 AM | |
Joined: 9/10/2021 Last visit: 3/2/2022 Posts: 4 Rating: (0) |
did you solve your issue? i face same kind of issues. please letme know solution |
Follow us on