(1)| 4/6/2021 12:32 PM | |
|
Joined: 7/26/2018 Last visit: 1/27/2025 Posts: 4 Rating:
|
Hello, I have installed the V2.6.1 image in IoT 2040. I have installed S7 node of version V2.1.1. IoT X1P1 port is assigned with 169.254.11.55 address & X2P1 is DHCP. S7 1200 PLC has IP address of 169.254.11.10 I don't have PLC hardware. I am trying to establish communication between IoT & S7-1200 by starting the S7-1200 in simulation but the communication is not established. Error is " Error connecting to PLC: Error: connect EHOSTUNREACH 169.254.11.10:102 " Can you suggest how to establish communication between the Simulation PLC(S7-1200) & IoT2040? Attached screenshot for reference ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/06/2021 14:17:10New subject after splitting |
|
Follow us on