1/27/2012 9:09 AM | |
Joined: 4/24/2006 Last visit: 3/28/2024 Posts: 8610 Rating: (1144) |
Dear Tomy Master, Perhaps this link might help: Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so? Best regards, Wizard |
2/5/2012 6:39 PM | |
Joined: 5/4/2009 Last visit: 7/29/2023 Posts: 914 Rating: (40) |
Would you please show me link for FAQ when using CP5611... |
Aim Higher |
|
2/6/2012 8:58 AM | |
Joined: 4/24/2006 Last visit: 3/28/2024 Posts: 8610 Rating: (1144) |
Hello Tomy, Please have a look at this link: What should you watch out for when setting up a connection between S7-200 and SIMATIC Panels or WinCC flexible PC Runtime and what are the options? See chapter 1. It is about profibus, but you can use it also when you use MPI. (So you should change it to MPI and a baudrate of 187,5) The PG/PC should be CP5611(MPI) Best regards, Wizard |
Follow us on