11/29/2020 8:44 PM | |
Joined: 9/27/2006 Last visit: 1/16/2021 Posts: 10353 Rating:
|
Hello; The document below explains how the S7-400 memory is organised and the options ypu have: How can I get an overview of the S7-400 memory concept? https://support.industry.siemens.com/cs/ww/en/view/7302549 The important points that could concern you are quoted here: Load memory: ... When using a RAM memory card (or integrated RAM memory),the system must be battery-operated so as to back up the RAM memory card data and the data in the internal RAM if there is a power failure. Note this last paragraph: the RAM memory, whether integrated as you will be using, or on a RAM memory card, is battery-supported. As long as you have a functional battery in the power supply module you can power down the CPU and maintain the program and data loaded in RAM memory. If the battery is depleted when you remove power to the CPU then you lose everything, your code and your data. - The battery you need can come from Siemens : 6ES7971-0BA00, SIMATIC S7-400, Backup battery 3.6 V/2.3 AH for PS 405/407,. - Alternative source for S7-400 batteries: SL 360 (Tadiran), www.tadiranbatteries.de/eng/home.asp Where can you find information about the S7-200/S7-300/S7-400 backup batteries? https://support.industry.siemens.com/cs/ww/en/view/12067424 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/29/2020 20:45:39 |
|
11/30/2020 7:11 AM | |
Joined: 12/8/2016 Last visit: 1/16/2021 Posts: 19 Rating:
|
thank you sir for good explain. i saw in a project that used internal memory and battery backup, and CPU doesn't have any BATTERY FAULT, but when we turn off the power , program lost and CPU will go to stop mode, i couldn't understand why. thank you |
Follow us on