8/18/2010 11:58 AM | |
Joined: 1/4/2010 Last visit: 7/2/2024 Posts: 650 Rating: (40)
|
Hi You know that windows 7 isn't compatilble with WinCC? http://support.automation.siemens.com/WW/view/en/21927773 also see this FAQ: Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x? |
Last edited by: Romulus at: 8/18/2010 12:01 PMRegards |
|
1/4/2011 11:09 PM | |
Posts: 14 Rating: (0) |
I have the same two issues on Windows Server 2003 R2 on which I installed WinCC 7 this week (except the run-time error number is-2147024769)) |
1/5/2011 8:29 AM | |
Posts: 799 Rating: (43) |
Dear GarryT, you should check if there is an "PDLPUBLISHINGWIZARD.log" in WinCC diagnostic folder (default: "C.\Programs\Siemens\WinCC\diagnose") Ich guess, that there are scripts in the pictures (pdl) which are not completely correct. (I hope that your error message is the same as in first post excepting the error number) best regards |
Last edited by: efka at: 1/5/2011 8:30 AM |
|
8/15/2016 1:52 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by ND120685 is split to a separate thread with the subject Web Navigator of PCS7 V8.1 Error. Best regards |
Follow us on