8/21/2018 11:23 AM | |
Posts: 6 Rating: (0) |
Hi Please visit my dropbox for 2 video's. https://www.dropbox.com/s/9fnhk31bqwz5l2p/20180814_110607.mp4?dl=0 https://www.dropbox.com/s/jj1hrdya70vxt1a/20180814_110731.mp4?dl=0 The Console, CRT and Power supply are from a GA3 control but all of the interface boards are from my original GA1 control. The result is the same if I have all of the boards in the GA1 frame with the original power supply. I hope this shows effectively what happens when I press the "ON" button on the NC machine panel. It shows the 3 led's on the front panel lighting up momentarily and the relay/s can be heard to click in and out. Then from the back, it shows the NC Fault light also coming on momentarily. |
8/22/2018 9:40 AM | |
Posts: 6 Rating: (0) |
Hi again, Sorry I forgot to say - Yes I have backup TEA1, TEA2,TEA5, PCA1, PCP1. Thank you, |
Follow us on