10/6/2020 9:48 PM | |
Joined: 8/10/2016 Last visit: 4/22/2024 Posts: 13 Rating: (0) |
Folks, I've got a few 840D SLs with embedded HMIs I wish to have a dialog displayed from the NC program. Ex, MMC("CYCLES,PICTURE_ON,T_SK.COM,SCREEN1,GUD.DEF,,,F1","S") I see there are several other topics along the same lines and I have found multiple documents that are getting me very close, however I am still missing something. https://cache.industry.siemens.com/dl/files/666/28820666/att_72845/v1/IAM_0106_en.pdf starting in section 4.5, among others but with the same information. I am attempting to re-create the examples just so I know how everything works. The problem I am running in to now is if I run that MMC command in an NC program, a screen pops up that says: The selected screenform was not found. The T_SK.COM file contains: //C1(SCREEN1) From the documentation I thought I understood that the .COM file needed to be in one of the NC data/Cycles folders however regardless of where I put the file (or if it even exists) I get the same screen. I suspect I am either putting it in the wrong folder or there's another step to setting this up somewhere that I am missing. |
12/17/2020 7:11 PM | |
Posts: 6 Rating: (0) |
HI Have you made any headway on this, I am trying to do the same Michael |
Follow us on