1/30/2014 8:40 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, check the data type of the variables which do you have defined. The parameters of the modules and the defined variables should have the same data type. See also the diagnostic FAQ with the function GET_DIAG. Perhaps you can find the error. http://support.automation.siemens.com/WW/view/en/75167627 With best regards |
7/17/2014 11:01 AM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoget the 8003 error code on the Homing logic block. With best regards, Narrator1
|
Follow us on