Industry Online Support
Technical Forum
9/10/2013 11:49 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello jebril The "AF" bit is not a Fault Condition. It is only a status bit indicating that Interrupts are enabled. Which is not a fault condition. When you say, "Machine is Stopping" , is your CPU in STOP or RUN ? If the CPU is in STOP Mode then press "F7 - Continue" to Display the next screen "Interrupt Stack" which displays the caus of interrupt ( WHy CPU went to STOP Mode ) If the CPU is still in run, then Please check your I/O signals for any sensor faults / I/O module faults ( If your program was working earlier with the same hardware ). Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on