7/16/2019 4:24 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Oleksandr; The following manual has some more details on the possible intyepretations of the As-i and Fault LEDs: System Manual AS-Interface (Edition 11/2008) with Supplements (Edition 09/2010 - for displaying and configuring see Entry ID 44365425) https://support.industry.siemens.com/cs/ww/en/view/26250840/6627327115 From your description it would seem that you are right in thinking the A-i slave address of the slaves is not recognized by the master. What method do you use to set the address on the As-i modules, an As-i addressing tool (see the link below) or the CP 342-2 addressing commands? I would recommend checking the As-i master to see if there is any limitation configured there, or the As-i slave addressing method. You do know that using a CP 343-2 allows you to implement As-i diagnostics, via OB 82? It will show As-i modules that are not present (or missing) in the master's configuration, and possibly some hints to restore them. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 07/16/2019 16:34:15 |
|
7/17/2019 8:38 AM | |
Joined: 9/21/2012 Last visit: 9/19/2024 Posts: 4144 Rating: (463) |
AS-i master v2.x doesn't have much you can configure in the HW. From AS-i v3.x -> there is more you can configure. Then there is also a "better" version of AS-i master 6GK7343-2AH11-0XA0, where you do internally the whole AS-i network configuration. What is the AS-i version of the new AS-i slaves? If they are V3.x, then there is a compatibility issue with the master. Even though the documentation declares that the new modules are downwards compatible with the older AS-i master versions, they might cause problems. |
7/17/2019 9:19 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
Unfortunately I only have 6GK7343-2AH00-0XA0 and i have to use it.
Where can I see the version 3RK1402-0BE00-0AA2? on the module, I see the symbol S3.0 - is it a version? old (existing ones that work correctly) modules have the same symbol S3.0 (photo attached)? |
Follow us on