Industry Online Support
Technical Forum
11/19/2010 7:16 AM | |
Posts: 53 Rating: (0) |
Dear All, 6ES72918BA200XA0 of S7-200? |
11/19/2010 7:27 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello Sreeram, Battery module for S7-200: A battery module is only an option for S7-200 CPUs. Here a high-performance capacitor handles data back-up in the case of temporary power failures. Only when the capacitor is empty do the battery module take over the power supply (see also Entry ID: 11868939). The back-up time of the capacitor depends on the CPU. Best regards, Hristo Mihalev |
11/19/2010 7:49 AM | |
Posts: 53 Rating: (0) |
Thanks a ton for the support which is very informative..... Regards Sreeram |
This contribution was helpful to1 thankful Users |
Follow us on