1/25/2016 2:25 PM | |
Posts: 14 Rating: (0) |
Hye all experts. A brief of my issue. I have PC/PPI cable for communicating S7-200. I tested the communication with CPU 224XP, which is a simulator that I bought, and I can establish the communication.The setting of the comm port, baud rate etc are as per normal ( but licsl address is 3,bot sure why).Remote address is 2. My laptop is using Win7 Ult, with Microwin 4.0 SP9. However when I tried to communicate with CPU 226, I could not establish any communication even with the same setting as above. Any advice? Rhis is strange, or can the original programmer blocked the communication? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/25/2016 4:06:51 PMNew subject after splitting |
|
1/26/2016 6:12 AM | |
Posts: 14 Rating: (0) |
hye Duris Update: Still unable to comm even when PLC is off |
1/26/2016 12:41 PM | |
Posts: 14 Rating: (0) |
I follow this,also failed. |
1/26/2016 5:20 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Picture of network parameters. |
With best regards... |
|
1/26/2016 8:51 PM | |
Posts: 14 Rating: (0) |
Hye William Port 1 to HMI. |
1/26/2016 8:55 PM | |
Posts: 14 Rating: (0) |
Duris This is the PCPPI. |
1/26/2016 8:57 PM | |
Posts: 14 Rating: (0) |
Hye Wizard It was programmed by someone else. by using PG, which cable ahould I use? |
1/26/2016 9:15 PM | |
Posts: 14 Rating: (0) |
This is CPU 224, and I managed to comm with it using the PCPPI |
Follow us on