6/14/2021 7:52 PM | |
Joined: 6/6/2021 Last visit: 9/18/2022 Posts: 9 Rating: (0) |
Sir actually i want to upgrade the handwheel which has selector switch am not getting the wiring diagram and am confused because the wire which is connected to X121 has only 11 connection in it and the mpg handwheel which i have purchased has 21 connection . If you have any solution then please let me know and it would be very thankful if you would give me any contact details of yours so that i can clearly get to know about it |
6/15/2021 5:17 AM | |
Joined: 9/6/2014 Last visit: 12/27/2023 Posts: 209 Rating: (6) |
Do you have any drawing about your new handwheel ? Normally before purchasing for exchange you must consider your plan ! Simply you need to compare any wires in new hardware with old and must define wires of MPG other than selector , then refer to electric document of your machine and find related connection ... . Selector keys for any system maybe differ because theirs as inputs for plc , so you must cheked your plc program . best regard |
6/15/2021 7:44 PM | |
Joined: 6/6/2021 Last visit: 9/18/2022 Posts: 9 Rating: (0) |
Sir actually they have giving colour code of wires thats it Sir should i send the wiring diagram of machine? |
Last edited by: Angad Jayant Walvekar at: 06/15/2021 19:46:58 |
|
6/16/2021 5:02 PM | |
Joined: 9/6/2014 Last visit: 12/27/2023 Posts: 209 Rating: (6) |
After last explain I think your problem must be solved but it seems you confused ! IF you are elementry for maintainance maybe dangerous for you or your machine ! please refer to skilled person closely ... . sorry and excuse me for above ! |
Follow us on