1/12/2012 1:20 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You can use the function Round to convert to DI and then convert DI to I. Or you download the Tips and tricks http://support.automation.siemens.com/WW/view/en/1232912 In Tip 38 is a Library included with 3 scale functions there you find one block Scale real to Int. See attached picture Regards, Marcjan |
Last edited by: Marcjan at: 1/12/2012 1:28 PMProblem solved? |
|
1/12/2012 1:28 PM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24)
|
hi first you have to use "R_TO_DI" instruction then "DI_TO_I" instruction. Alternatively you can use "ROUND" or "TRUNC" instead of "R_TO_DI". "DI_TO_I" is always necessary. See manual http://support.automation.siemens.com/WW/view/en/1109582--> page 100,101 regards |
1/16/2012 7:59 AM | |
Posts: 6 Rating: (0) |
Thank you very much |
This contribution was helpful to2 thankful Users |
1/18/2013 9:40 AM | |
Posts: 79 Rating: (7) |
Simply use SCALA library R to I, just enter limits & enjoy. |
Follow us on