Industry Online Support
Technical Forum
4/2/2011 6:43 PM | |||
Posts: 11 Rating: (0) |
Dear Simaticmanager, Could send me the exact converter configuration beacuse there are two configuartion posted by sevab peter i.e V24-TTY.pdf in which there is no connection of pin 14 and the other one is alfie i.e Cable for CP to program with a 6ES5734-1BD20.pdf in which 14-12 are connected from CPU.I am confused which one is correct .I am using the siemens cable PC /TTY Cable ( 6ES5 734-1BD20 ) and in the V24-TTY config ,there is no clearity of both Connecter beacuse in second config one is DB 25 and other one is DB15 so my problem is 1. how it is connected to PC/TTY cable ? without removing DB15 to TTY part 2.Is the V24-TTY both the connectos ar DB 15 so i can use it after my PC/TTY means CP+conversion cable + PC/TTY cable Please reply as early as possible Splitted from communication between cp143 and pg. AttachmentCable for CP to program with a 6ES5734-1BD20[1].zip (156 Downloads) |
||
Last edited by: O_Moderator at: 4/5/2011 10:12 AMnew subject after splitting |
|||
Follow us on