10/4/2020 12:30 PM | |
Joined: 12/6/2010 Last visit: 3/12/2024 Posts: 6 Rating: (0) |
Dear ALL I have uploaded attached program from runinig S5 system Now i whant to convert into S7 using S5 converting tools. However,when I try that,I find lotof warninig and &error. I can live with the warning but errors are not allowing to convert the program. Can anybody help me out in this? I HAVE attached s5 progrme. Wait for some helpful resoned. Attachment13322_V3_SIMATIC_S5.zip (249 Downloads) |
10/4/2020 1:55 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32847 Rating: (4061) |
If we had this theme at last, I refer to this topic: But I want to a look at your S5 file ... |
10/4/2020 2:24 PM | |
Joined: 12/6/2010 Last visit: 3/12/2024 Posts: 6 Rating: (0) |
H ELLO MY S5 PROGRAMIS IN THE ZIP File. I Have the convet and know how to used him. But my problem is that I dont know how to fix the Error. THANEKS Attachment13322_V3_SIMATIC_S5.zip (191 Downloads) |
10/4/2020 2:50 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32847 Rating: (4061) |
The problem is the S5 program use instructions the are not can converted to S7. LIR = Load the register indirectly See attachment of a print of FB210 from the S5 file. Attachment13322ALS.pdf (220 Downloads) |
This contribution was helpful to1 thankful Users |
10/5/2020 7:02 AM | |
Joined: 12/6/2010 Last visit: 3/12/2024 Posts: 6 Rating: (0) |
THANEKS |
This contribution was helpful to1 thankful Users |
Follow us on