6/15/2019 1:50 PM | |
Joined: 12/17/2011 Last visit: 3/5/2024 Posts: 7 Rating: (2) |
Hi masters, I have CPU 3152DP with additional new profinet CP 343-1 and unsolved problem with diagnostic via FB126. I have tested also RDSYST SFC51, but have same result- nothing CALL SFC 51 REQ :=TRUE SZL_ID :=W#16#591 //SZL_ID for the state of the IO devices 591 INDEX :=W#16#64 //number of the PROFINET-IO system (hexadecimal) RET_VAL :=DB50.DBW4 BUSY :=DB50.DBX6.0 SZL_HEADER:="DIAG_STRUCT".SSL_HEADER DR :=P#DB60.DBX0.0 BYTE 258 //data record with diagnostic information project in attachment. AttachmentG7971871.zip (35 Downloads) |
Last edited by: Chive at: 06/15/2019 13:55:56Last edited by: Chive at: 06/15/2019 13:58:41Last edited by: Chive at: 06/15/2019 14:01:42 |
|
6/17/2019 4:36 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046)
|
Hello Chive as far as I know, S7-300 CP's are NOT supported by PNIODiag FB126 (and probably never will, but am happy to stand corrected on this one). See also the pdf that is part of Entry ID:98278878 which details what S7 300 CPU's and S7 400 CPU (as well as some of S7 400 CP's) are supported. |
Last edited by: Jen_Moderator at: 06/17/2019 10:03:00Optimized link. Cheers |
|
10/14/2020 12:01 PM | |
Posts: 9 Rating: (0) |
Hi man, did you already solve it? I have a same problem and I need to know, if there is some solution. Thx |
Follow us on