4/10/2012 5:54 PM | |
Posts: 133 Rating: (2) |
It shows some write/read error (ID#2523,2522) which need OB121,but nothing about PROFIBUS; those errors DOESN`T force CPU in STOP |
4/10/2012 9:59 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? |
4/10/2012 11:01 PM | |
Posts: 133 Rating: (2) |
the only OB that i didn`t download is OB83, tomorrow i will try, and if doesn t work i `ll post a screen shot of it (project too large for size forum) |
4/11/2012 8:10 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
In future you can contact withModeratorand ask for help in case of attachment exceeding allowed bytes. Best regards, Hristo Mihalev
|
4/11/2012 11:06 AM | |
Posts: 133 Rating: (2) |
I can t download OB83 to CPU, step7 says me "can t copy..." ; CPU3152DP |
4/11/2012 12:20 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
OB83 is not support for your type of CPU. Best regards, Hristo Mihalev |
4/11/2012 12:46 PM | |
Posts: 133 Rating: (2) |
So it isnt OB83 to cause CPU STOP |
Follow us on