8/7/2019 1:25 PM | |||||
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33790 Rating: (4197) |
With this information, the Drive ES Drive ES Basic Maintenance product V5.6 SP2 product is released for delivery effective July 26, 2019. Drive ES Basic Maintenance product V5.6 SP2 is released for delivery with this information. Ordering information about Drive ES Basic Maintenance V5.6 SP2. Drive ES Basic Maintenance V5.6 SP2 replaces the previous version V5.6 SP1, which means that the Article number remains unchanged.
Reasons for revising and ongoing development include the actualization of the integrated project manager and the SimoCom U commissioning tool to V14.03.02 and SimoCom A commissioning tool to V05.05.04 - as well as the update of the supported Microsoft operating systems. The previous Drive ES Basic Maintenance V5.6 SP2 version was innovated to include the following new features (unchanged tool versions are also listed):
Advantages of a Drive ES Basic installation compared to the installation of individual tools
The integrated commissioning tools can also be individually downloaded from the Internet and can thus be used as a free upgrade for an existing Drive ES Basic (Maintenance) installation from V5.4 SPx (V5.6 SP2):
How can I obtain the new Drive ES Basic Maintenance version?
Hint according usage at SIMATIC PCS 7;
Operating systems and STEP7 compatibility Drive ES Basic Maintenance can be used with the following Microsoft operating systems:
Drive ES Basic Maintenance V5.6 SP2 can be used with the following STEP7 versions (minimum precondition):
Detailed information on the compatibility is provided in 18495518 Supported languages
Note Drive ES Basic Maintenance can only be installed additionally as a pure option package for the SIMATIC STEP7 full Version. |
||||
Last edited by: Jen_Moderator at: 08/08/2019 08:43:14Optimized links. |
|||||
This contribution was helpful to1 thankful Users |
Follow us on