7/11/2016 2:33 PM | |
Posts: 24 Rating: (1) |
Dear Experts, I would like to know the differences between CPU 410 and CPU 417. Thank you. |
7/11/2016 2:53 PM | |
Joined: 7/9/2015 Last visit: 4/19/2024 Posts: 3809 Rating: (554) |
Hi, please check the technical Data of your PLCs: SIPLUS PCS 7 CPU 410SIPLUS_CPU_417Regards, Towome |
|
|
7/11/2016 3:54 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664)
|
Hello jigarhg; Along with Towone's links to the technical data of the standard S7-400H CPUs (represented bu the S7-417H) and the new S7-410-5H, here are 2 documents that explain how the CPU 410 represents a new approach to process control, with PCS 7 v8.x and higher, replacing the CPUs S7-417H (and lower) in PCS 7 projects. The CPU 410-5H is a scalable process controller unit that can be adapted (with special System Expansion Cards) to various numbers of PO (Process Objects), instead of tag numbers. A Process Object can be a motor, or a PID, or a compressor, with all the required input , output and internal tags required to control and monitor it. The smallest number of POs available is 100, and goes up to "unlimited" (if ever required) by increments of 100 or 500 POs. Have a look here for initial information: https://support.industry.siemens.com/cs/de/en/view/74736822 https://support.industry.siemens.com/cs/de/en/view/96839331 CPU 410-5H at a glance In this chapter you will find general information on the CPU 410-5H, its functions and areas of application. Introduction The CPU 410-5H is a controller specially designed for process automation which is versatile in use. With its robust, high performance hardware, the CPU 410-5H covers the entire performance spectrum of the AS 412 to AS 417 complementary systems. Scalable performance The performance range of the CPU 410-5H can be individually scaled according to the size and type of the PCS 7 applications. This is done by means of the PO volume, which is determined by the System Expansion Card (SEC). The volume extends from 100 PO to unlimited, at which point other performance data of the CPU act as the limiting factor. The PO quantity structure of an SEC can be conveniently extended from the PCS 7 V8.1 by means of CPU 410 expansion packs. It is not necessary to dismantle the CPU or the SEC. There are CPU 410 expansion packs available for 100 POs and 500 POs. Hope this helps, Daniel Chartier |
This contribution was helpful to5 thankful Users |
Follow us on