12/24/2015 11:09 PM | |
Posts: 101 Rating: (1) |
If i switch the Master for CPU0 To CPU 1 and download the Programms Normaly It can be Helpful No? |
12/25/2015 12:28 PM | |
Posts: 101 Rating: (1) |
plz how can i change the target systeme to the other cpu via simatic ,we have one staion with two cpu 414-4h all programms are in the first cpu |
12/25/2015 12:54 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
If you have an intact redundant system , that would not be the case .Buffer of both CPUs will be the great evidence to judge .In order to select the target system , check the attached file. Attachment2.rar (116 Downloads) |
12/25/2015 2:55 PM | |
Posts: 101 Rating: (1) |
Yes ,This Taget is For dowload The Configuration I will Dowload It To the CPU 1 OKK And After That I download All Programms Normally in The Station ?? |
12/25/2015 3:07 PM | |
Posts: 101 Rating: (1) |
1 --I will dowload the HW in CPU 1 2-- I dowload all Programms normally AttachmentCPU414.rar (100 Downloads) |
12/28/2015 8:13 PM | |
Posts: 101 Rating: (1) |
Finaly the Problem was resolved by a simple manipulation its just to choos the hole station-H and make a dowload and make the target to the CPU1 :) |
Follow us on