Industry Online Support
Technical Forum
10/4/2014 10:31 AM | |
Posts: 56 Rating: (2) |
what is the type of encoder used ? |
10/4/2014 9:08 PM | |
Posts: 11 Rating: (0) |
Is a absolute encoder, SICOD, model Z65-G-512-824-B-CV. |
10/6/2014 8:29 PM | |
Posts: 11 Rating: (0) |
The machines were running, were sold off, came to Brazil and were mounted. What happened was that the battery died, was replaced and reinstalled the program on both machines. One worked the other did not. How do I monitor the program the encoder signal? I'm sending attachments programs, since we have two CPU's in the rack. grateful.
AttachmentAsten.zip (69 Downloads) |
10/8/2014 10:07 AM | |
Posts: 56 Rating: (2) |
Kindly try to program the Encoder Zero position of the system.If absolute encoder position got disturbed also this problem may come . |
Follow us on