1/18/2022 10:43 PM | |
Joined: 9/8/2021 Last visit: 4/24/2024 Posts: 3 Rating: (0) |
Hi, I am trying to go online with all the nodes on my Profibus Network. I am online with my ET200 Pro on the network on Step7 Simatic Manager Hardware Configuration. (For example: Node 11 Bay 3 is online on the Profibus Network but when I look into the individual module on the ET200, the module are greyed out which I assume are not online (Picture 2) . I tried to manually set the input for the module at Slot 4 (8 DI DC 24V HF). I could see the green light on the that particular module Input on ET200 but not on the Step 7 Simatic Manager Status Value (For example: I set Input 14.0 "Sta05_GT2_PassBit" to true, the green light on the module is On but not on the Status Value on the Software. Picture 3). I am just a beginner and not sure what could be the issue. The physical module and its order number also matches with the one on the hardware configuration. Thank you in advance. AttachmentPictures.docx (249 Downloads) |
Follow us on