2/5/2017 10:24 AM | |
Joined: 8/25/2006 Last visit: 4/24/2024 Posts: 2203 Rating: (277)
|
Hello. There is no any manual available for downloading, only this info. When you will buy this product you will get all the manuals with it. |
This contribution was helpful to1 thankful Users |
2/5/2017 11:32 AM | |
Joined: 8/25/2006 Last visit: 4/24/2024 Posts: 2203 Rating: (277)
|
Make a Support Request with product order number, I think technical support will give you all answers. |
This contribution was helpful to1 thankful Users |
2/6/2017 6:39 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello ---- The FM 458-1 DP Know-How Protect module enables protection of technological user function blocks against unauthorized copying. The FM 458-1 DP Know-How Protect module can prevent that a FM458-1 DP configuration with user function blocks is copied and used for further systems or projects. All user function blocks created with the D7 function block generator can check with their system function whether a FM 458-1 DP Know-How Protect module is plugged into the rack, and whether the latter has the correct identification. The response in the case of a missing FM 458-1 DP Know-How Protect module, or if the identification is incorrect, can be predetermined for each user function block individually. ----- This essentially means that you can only protect the blocks which are created using D7 FB Creator, from being run in unauthorised enviornment ( Not haing the matching Dongle ) Hope this helps |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on