11/24/2014 2:02 PM | |
Posts: 24 Rating: (8) |
If you are storing your project on a network drive and multiple programming stations are trying to access it, there will be an additional problem with the help files if you have the latest Windows 7 (32 or 64bit) work station. Basically, Microsoft abandoned the "help" platformthe TDC help fileswere developed with seemingly due to security risk by virus attack. To get these files to work again, WinHlp32.exe must be reinstalled per Microsoft instructions found on their website: http://support.microsoft.com/kb/917607#3 A Windows Registry entry also has to be made to allow the help files to be opened over the network. Instructions for doing this are below. Fixing the SIMATIC Help file Read Problems on the new Programming Station: 1. Log on by using an administrator account. 2. Press the Windows logo key + R, type regedit, and then click OK. On 64-bit editions of Windows, locate and then select the following registry subkey: HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Microsoft 3. On the Edit menu, point to New, and then click Key. 4. Type WinHelp, and then press Enter. 5. Click the WinHelp key. 6. On the Edit menu, point to New, and then click DWORD (32-bit) Value. 7. Type AllowIntranetAccess, and then press Enter. 8. On the Edit menu, click Modify. 9. In the Value data box, type 1, click Hexadecimal in the Base area, and then click OK. |
This contribution was helpful to1 thankful Users |
Follow us on