9/13/2019 12:33 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645)
|
Hello first you need a trigger. SO you have to use one of the interface Properties you use in the Script with it´s event Value Change -> then you have to start the script. -> then use an Animation or appearance on the rectangle -> and use here a faceplate internal tag -> Then create the Script and use the preudo code you have postet (in correct VB Syntax of course). If you need help in scripting: https://support.industry.siemens.com/cs/ww/en/view/59885894 Bye Murof |
Last edited by: Murof at: 09/13/2019 12:34:22If this Information really helps, you could use the Rate function |
|
10/2/2019 1:55 AM | |
Joined: 11/23/2007 Last visit: 4/12/2024 Posts: 117 Rating: (3) |
In faceplate in comfort panel I can't launch script with value change. It's my problem |
10/2/2019 5:28 PM | |
Joined: 11/23/2007 Last visit: 4/12/2024 Posts: 117 Rating: (3) |
Yes I have a script in my faceplate but i can't launch it because in i/o field i can't program an action in i/o filed |
Follow us on