9/24/2014 4:04 AM | |
Posts: 14 Rating: (0) |
I readed this manual, but i don't have this setup file, could you send me this file or give me the link of 802d toolbox. |
9/24/2014 5:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
This file is available in tool box CD. Please contact Siemens for the same. |
9/24/2014 6:35 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
When you are reloading the back up, needs to connect with drive, MCP, KEY BOARD, PP module. |
10/21/2014 5:35 AM | |
Posts: 14 Rating: (0) |
Dear Mr PISCEAN 2010! I try as you said: I connect everything to sinumrik then first i download file settup_T, it success, then i download my startup file, my pc send success, but on sinumerik has transmittion error (image P1) : _N_CYCLE383T_SPF; PATH =/_N_CST_DIR OK Error! Code: 0x58 And on alarm windown has some error (image p2): 026015 Axis z1 machine data mn_drive_telegram_type[1] invalid value 026015 Axis x1 machine data mn_drive_telegram_type p915[0] invalid value 026015 Axis z1 machine data mn_drive_telegram_type p915[0] invalid value So i check machine data and found that all parameter 13060 drive_telegram_type are 0 (image p3), then i set those to value 102 and 104 (image p4) save and reset sinumerik, and there are no error remain, then i try to run machine every thing ok, drive x, z and spindle run ok, there no error occur but the spindle speed feedback no speed and on sinumerik has message Wait spindle (image p5) I replace spindle encoder but not success, i online simodrive 611 using simocom U and i can see encoder data change on profibus diagnostic frame, so i think my encoder is ok. My machine have 1 double motor module for drive X and Z axis, and spindle encoder is 6fx2001-2eb02 , it connect to X472 I guest parameter 13060 are not correct, so please help me setting correct machine data parameter Attachmentimage.zip (201 Downloads) |
10/26/2014 8:47 AM | |
Posts: 14 Rating: (0) |
in my machine par13070 is set 0f, now i must set it to 8000h? i read in manual 8000h mean deactive consistent check of profibus telegrame. is this right?
|
Follow us on