6/24/2020 12:00 PM | |
Joined: 1/18/2016 Last visit: 11/27/2022 Posts: 8 Rating: (0) |
Hello. I have problem with MC_GearInPos. I configure this block and with parameter SyncProfileReference = 1, the Slave_Axis doesn't start, but in functional block output parameter Busy = 1. When I set SyncProfileReference = 0 slave _axis also doesn't start, but i've got error detail "608", reaction "2". With MC_gearIn I don't have such problems, except I need to program Flying Saw and cut with accuracy = +- 1mm, with GearIn I have accuracy about +-20mm. Help me to program GearInPos Here attachment what I programmed ------------------------------------------------------------------------------------------ |
Last edited by: vagan at: 06/24/2020 12:04:04Last edited by: Jen_Moderator at: 06/24/2020 13:22:20New subject after splitting |
|
6/29/2020 9:40 AM | |
Joined: 4/28/2015 Last visit: 10/20/2023 Posts: 43 Rating: (6) |
Please also have a look at SIMATIC S7-1500(T): Comparison of the synchronization modes |
Grüße, Axel |
|
Follow us on