4/25/2016 4:01 AM | |
Posts: 78 Rating: (0) |
I have started a new job running a Lathe with old (late 1990's early 2000"s) seimans 840D control. At the moment I'm using existing programs and trying to understand them .I'm hoping someone could explain why the below program needs two different offset pages to work .T2D2 offset page has two length compensations in it where as T2D3 has three and I’m not sure what the third one is for. I have attached an example of the different offset pages that I copied from the manual. If someone could explain what the third compensation is used for that would be great T2 D2 ;FORM TOOL POSITIONING N840 M6 N850 G0 X10 N860 Z-7.5 N870 N880 T2 D3 ;FORM TOOL MILLING N890 M6 N900 G17 N910 G94 N920 S2=1000 M2=4 N930 SETMS N940 SPOS=180 N950 DIAMOF N960 TRANSMIT N970 ROT RPL=-180 N980 G1 G42 X-6.4 Y-14 F300 N990 Y14 N1000 G40 X31 N1010 G0 X70 N1020 DIAMON N1030 TRAFOOF N1040 G18 N1050 M2=5
Attachmentoffset page.docx (130 Downloads) |
4/25/2016 9:35 AM | |
Posts: 78 Rating: (0) |
Thanks PISCEAN I'm still a bit confused with the whole setup but with try and write some test programs next week which may make things a bit clearer |
5/12/2016 11:06 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:09:31 AM~(‾▿‾)~ |
|
Follow us on