10/30/2016 3:38 PM | |
Posts: 3 Rating: (0) |
have motor 1fk7083-5af71-ug3-z connected to driver SINAMICS S120 when it run there is high temperature i used starter software to monitoring i see ampere is normal in attached the file upload from the drive the drive name Drive_Cream i hope anyone can help me to solve this problem Attachmentuploud.zip (96 Downloads) |
11/6/2016 6:40 PM | |
Posts: 3 Rating: (0) |
thank for your kindly replay i measure the motor temperature by starter software and use infrared sensor the temperature more than 100 c |
Follow us on