12/13/2019 11:03 AM | |
Joined: 3/5/2017 Last visit: 4/16/2024 Posts: 769 Rating: (126) |
Hi, I don't think it is possible to do that, even with a script. You can check if SD card is available or fullwith a script. Someone please correct if i'm wrong. You would need to make an external program to WinCE, then it is possible. I would not recommend to learn to do that. Only thing that comes in mind is to use Audit trail. It needs a licence to use, so that is not good option. But when i tested, i noticed that when you don't actually log anything and just use it to check SD status, it won't complain about the licences. Licence complaint should come right after you power on panel. Test if you want. Attached steps to activate Audit trail AttachmentLowMem.pdf (335 Downloads) |
Last edited by: K_Ohjus at: 12/13/2019 11:08:15Last edited by: K_Ohjus at: 12/13/2019 11:17:36Last edited by: K_Ohjus at: 12/13/2019 11:18:25- Trying is the first step towards failure. |
|
12/16/2019 2:01 AM | |
Joined: 4/18/2014 Last visit: 3/25/2024 Posts: 253 Rating: (5) |
And kindly share the back up if any one have tia v14 software. Regrds, GUWS |
Last edited by: GUWS at: 12/16/2019 02:21:55Last edited by: GUWS at: 12/16/2019 03:56:50 |
|
12/16/2019 4:33 AM | |
Joined: 4/18/2014 Last visit: 3/25/2024 Posts: 253 Rating: (5) |
|
Last edited by: GUWS at: 12/16/2019 04:34:06Last edited by: GUWS at: 12/16/2019 04:34:45Last edited by: GUWS at: 12/16/2019 04:36:59Last edited by: GUWS at: 12/16/2019 05:22:04Last edited by: GUWS at: 12/16/2019 05:22:22Last edited by: GUWS at: 12/16/2019 05:27:20Last edited by: GUWS at: 12/16/2019 05:45:21Last edited by: Jen_Moderator at: 12/16/2019 06:29:09Optimized link. |
|
Follow us on