6/11/2019 4:09 AM | |
Posts: 2 Rating: (0) |
i also have similar problem. i am trying to scale temperature. my min. and max. temperatures are 20 and 800 degrees respectively. i want to control the temperature to not greater than 250 degrees and not less than 40 degrees. how can i do the scaling without using the normalized value of 0.0 and 1.0? i want to use the temperature values. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/12/2019 13:31:58New subject after splitting |
|
6/13/2019 12:56 PM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
You can use the scaling formula = out_max - out_min( in - in_min )/in_max- in_min + out_min Just feed it with the values you need at the output and inputs that you feed and will give you your desired output |
Thanks and Regards |
|
This contribution was helpful to1 thankful Users |